11/29/2007 5:42 PM | |
Joined: 10/31/2007 Last visit: 1/21/2025 Posts: 7 Rating:
|
I cleaned the CPU and back plane along with the other moduals in the system. I reladed the software and came up with the same issues. I do not have a spare to swap out at this time our other machine is in use 24x7. The errors also show up when trying to compair blocks. I have attached the compair file and the ladder blocks so mayby you could take a look to see if I am over looking something. Thanks Jeff Attachment810m_plc_problem.pdf (618 Downloads) |
Follow us on