8/4/2023 8:55 AM | |
Joined: 1/21/2013 Last visit: 3/28/2024 Posts: 2616 Rating: (420)
|
Hi Martijn, Unfortunately, even though the sorting of alarms has been improved, there are still some open issues for the developers. A few notes about V18 Update 2 - as with every update. In most cases there are more components to update.
Although the ES and device versions should only change when new functionality is required, it might be helpful to install this as well if only some runtime fixes are needed. This will keep you close to the system that development uses for most testing. If all updates do not solve the problem, you should create a new support request. This will ensure that the developer will also look into your use case. Kind regards |
Follow us on