12/9/2010 3:12 AM | |
Joined: 6/5/2009 Last visit: 3/17/2025 Posts: 153 Rating:
|
Hi Mr.J_Bell I use Step 7 version 5.4 SP5. By the way the .hfg file version 2.0 is available for CP 343-1 Lean. I need to use v2.3 for the hardware that I've got. But in the hardware catalog I have only v2.0 as the last. I need the configuration file for the same. By the way the service that is used here is Industrial Ethernet. All tags are configured under Industrial Ethernet. The mode of communication is Ethernet (which is obvious) and IP addressing is used for communication.
|
Follow us on