11/13/2017 9:16 AM | |
Posts: 167 Rating:
|
Hi, I`m thinking using Stahl ET-208, see attached datasheet. [snip] ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/15/2017 7:55:46 AMDeleted 1st quesiton. Last edited by: Jen_Moderator at: 11/15/2017 8:18:34 AMInserted remark. |
|
11/14/2017 8:54 AM | |
Posts: 167 Rating:
|
I will give you full information. I only have to pair to use from the cabinet to the panel in the field. Project 1: Project 2:
2. What must I do, to be able to connect wo ET-208 panels to the same MPI port. AttachmentSDS_OS ET-208-TX_en-GB.pdf (136 Downloads) |
Last edited by: Jen_Moderator at: 11/15/2017 7:53:53 AMDeleted 1st question. |
|
11/14/2017 9:51 AM | |
Posts: 167 Rating:
|
Thank you, I sent them a email these morning so lets see I can update you if you are interest. |
This contribution was helpful to
1 thankful Users |
Follow us on