7/28/2020 9:30 PM | |
Joined: 12/4/2014 Last visit: 1/26/2023 Posts: 11 Rating: (0) |
Hi, I successfully applied the above method for square wave type velocity profile. Now I need to perform arbitrary time-dependent speed profile. Do I need to use any Technology Object of the drive or PLC. The final axis to be speed-regulated is on the motor shaft and feedback element is the encoder on the motor shaft. Do have any recommendation for high-performance speed control? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/29/2020 09:12:50New subject after splitting |
|
Follow us on