1/24/2015 8:15 AM | |
Posts: 81 Rating: (0) |
Hi Friends, Is there anyway that we can set the PLC to stop button using a tag of bool type, when the tag triggers the PLC should go to STOP mode. Thanks, pavan.
|
1/24/2015 1:37 PM | |
Posts: 84 Rating: (19) |
Hi, If you have a Simatic HMI you can change and monitor the PLC mode
|
1/24/2015 5:24 PM | |
Posts: 81 Rating: (0) |
Hi subin, I need to do it based on a tag value of PLC, if that sets to 1 PLC should go to STOP mode and if it goes to 0 PLC should go to run mode Thanks |
1/31/2015 1:06 AM | |
Posts: 34 Rating: (1) |
I would be looking at using a timer to kill the power to and from the machine during sleeping hours rather than relying on the CPU to do the job for you. |
12/20/2017 7:35 AM | |
Joined: 6/19/2017 Last visit: 4/25/2024 Posts: 7954 Rating: (162) |
New question published by KAMY is split to a separate thread with the subject Is there a way to program CPU so that it goes to stop mode and motor color will be disable?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on