6/22/2023 1:10 PM | |
Joined: 9/12/2017 Last visit: 9/22/2023 Posts: 2 Rating:
|
Dear Pegaia, I tried out your project and it works fine on PC RT. I need to realize the audit functionality on UCP, but it does not work... I just changed some things that is neccessary to work on UCP, like the path of the export file (media/simatic/X61/). The WriteFile function create the exported.csv file on the USB (X61) , but it contains only the header text. (TimeStamp,AuditProviderType,ObjectReference,etc...) I use V17 Upd5. I read that audit supported on UCP from V17 Upd1. Are there any settings that I need to set on UCP compared to Unified PC? Thank you in advance! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/23/2023 07:55:21New subject after splitting |
|
Follow us on