4/16/2019 9:19 PM | |
Posts: 18 Rating:
|
Hi, i am also looking for a solution because i need to setup communication with the IT Network in a factory using ISO onTCP My Configuration : CPU F1518-4PN (10.89.0.199 / 255.255.255.192) PUT/GET activated CP 1543-1 (10.89.0.200 / / 255.255.255.192 / Router= 10.89.0.193) FETCH/WRITE activated i use the FB "TSEND_C" to manage the connect / Send / Disconnect with the IT PC Partner And it's not working, the STATUS is blink between 16#7001 and 16#7002... my question is also to know if i have to put the local TSAP (TSAP of the CP card in the "TSAP list") and if i want to add the receive FB 'TRCV_C", i need to create à new link for the connexion data with an other connexion ID number ? Thanks in advance for help because the documentation is not clear on this point ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/17/2019 10:20:25 AMNew subject after splitting |
|
4/17/2019 2:12 PM | |
Posts: 1368 Rating:
|
Hello, code 7001 and 7002 is no error. it means, the block is waiting for request or is working at the moment. |
Follow us on