2/14/2016 8:29 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
hellu guy; What version of DIGSI have you installed? For example DIGSI 4 (v4.84) installs on Windows XP SP3 32-bit. See the following document: digsi 4 - Siemens Other versions will have their own OS requirements. Hope this helps, Daniel Chartier |
2/14/2016 9:51 PM | |
Posts: 12 Rating: (0) |
Hi. You can see that in the topic description. It says DIGSI 4.88 Okay, thank you. I can see in the document that 4.88 should support XP SP 3, and that is what I have installed. It does run on Windows Virtual PC though, but should it matter? My driver installation wizard asks for a .inf file, and it is not provided apparently. |
Last edited by: e-guyatwork at: 2/14/2016 9:55:09 PMLast edited by: e-guyatwork at: 2/14/2016 9:55:32 PM |
|
2/14/2016 10:33 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello guy; Well, installing any software in a virtual environment requires attention to the VMware version details and prameters. For example: From the DIGSI 4.88 Installation Notes Virtual Environment DIGSI V4.88 supports the virtual environment VMware in the following versions and higher: • VMware Workstation V6.5.0 • VMware Player V3.1.2 • VMware Tools for Windows V8.4.4 (For more information, see http://www.vmware.com). And another thread on the forum shows the problems of a DIGSI user with his serial drivers: (Our friend MikeJ gives some useful information on this problem) https://support.industry.siemens.com/tf/ww/en/posts/51937/ Hope this helps, Daniel Chartier |
2/14/2016 10:48 PM | |
Posts: 12 Rating: (0) |
Thank you Daniel. The problem is the driver, not the software. I am just using USB to USB connection, and without DIGSI started, I am trying to first install the driver so that windows can recognize the device, but it cannot. Digsi is working fine, but the driver for windows XP is not working. It detects Siprotec 4 device, but it does not have the driver for the device. |
Last edited by: e-guyatwork at: 2/14/2016 10:49:35 PM |
|
Follow us on