5/24/2018 4:53 AM | |
Posts: 1283 Rating:
|
Hi all, My problem is that i was not able to copy files from the HMI folder to Network drive. I can save data logs in Network folder, but unable to copy anything to the network folder using scripts, In the images attached, i had assigned data logging in network folder which works fine. but when i try to copy the same from the network folder to another location inside the same network folder, it says it cannot find the network path. I can use the same script for USB data logging and copying, it works fine. the problem is that the network folder is not visible in the HMI network folder can access manually the network folder using file explorer, but copying through the scripts doesn't work. it says the specified path doesn't exist. Hope some one can help. thanks in advance, jay AttachmentNetwork folder.docx (179 Downloads) |
6/7/2018 3:47 PM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15355 Rating:
|
Hello Jaya perhaps this FAQ can help: https://support.industry.siemens.com/cs/de/en/view/109742375 And of course check the Basics: https://support.industry.siemens.com/cs/ww/en/view/92346478 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
6/7/2018 5:06 PM | |
Posts: 1283 Rating:
|
Thanks a lot Muro. Straight to the point and exactly what I am looking for. Thanks again. Jay |
This contribution was helpful to
1 thankful Users |
Follow us on