11/14/2009 2:42 PM | |
Joined: 7/18/2006 Last visit: 2/6/2023 Posts: 28 Rating:
|
I have following proposed networkconfig. for our one of upcoming project. We are fetching S5 data through old OTN -36 network via MTU interface (using ethernet S5 CP) to our new proposed pcs7 system via optical fiber connected to scalance.(we dont want to use Old LSX top end instead we are proposing pcs7 sytem at top end.Please refer to network configuration. we are also simultaniously communicating to pcs7 system from our new RTUS7-400H stations. Can anybody tell me their views on this network?? any better solution??? this is S5- pcs7 migration project which we are doing in phase manner. Later all s5 nodes will be discarded and new s7 stations will take over. Regards Ushu. Attachmentnetworkconfig.pdf (39 Downloads) |
Follow us on