2/1/2022 3:14 PM | |
Joined: 4/12/2016 Last visit: 11/27/2023 Posts: 19 Rating:
|
I wish I had read the complete text before upgrading the FW to v1.2.1, because now my eMMC is loaded with an old image which is not compatible with the new firmware and there is no way to load in to the OS any more to change the boot order...arggghh. I have read other users struggling with the same, how to get rid of the image on the eMMC? Not possible? I connected the UART but just stops and hangs (see attached). It says hit any key but how to stop te auto boot? It does not respond to the keys from the USB keyboard and continues booting from the eMMC which is not working. Is there any way how to solve this? other question, how to find any release notes on the example images/firmware? Thanks. regards, Remco Attachmentboot.txt (233 Downloads) |
2/1/2022 4:43 PM | |
Joined: 4/28/2015 Last visit: 12/1/2023 Posts: 3294 Rating:
|
Hi, you were too fast. I was about to post something about the update here in the forum Best regards! |
Follow us on