9/23/2008 2:38 PM | |
Posts: 103 Rating: (10) |
Were you logged in as an Administrator when you installed the software? Are you trying to access a folder now that requires Administrative rights? |
9/25/2008 9:49 AM | |
Posts: 81 Rating: (0) |
Yes, I am using the DVD Microsoft SQL Server 2005 Service pack1 for Wincc 6.2 |
9/25/2008 4:26 PM | |
Posts: 487 Rating: (44) |
This is a strange problem. So we have to look at all possible problems. Is the machine part of a domain? Is the network card not connected at all? Did you change PC name after installation of SQL sever? Take a look at this FAQ, there are many problems discussed under this, though the symptom is a bit different. May be worth a try. http://support.automation.siemens.com/WW/view/en/23711489 |
9/26/2008 10:05 AM | |
Posts: 81 Rating: (0) |
More Information: Wincc Diagnose: 2008_9_26 8 8:57:58:944 CCProjectMgr.exe CSingletonProject::AttachDatabases pICCDBManagement->AttachDatabase \\IESCRK-C052\WinCC60_Project_hi\hi.mdf on IESCRK-C052 failed: 0x8004d903 Regards |