7/25/2007 3:05 PM | |
Posts: 3149 Rating:
|
Hi |
7/26/2007 12:26 PM | |
Posts: 9 Rating:
|
Hi I have attached all files from the \wincc\diagnose catalogue. The problem occured after 17.july. We have detected that the CPU load of the OS (OST1) goes to 100% (and stays there), while trying to "fill faceplate" with dynamic data. We also have tried to start the runtime application from the engineerings station (ES1). We get the same result; opening faceplates makes the CPU go in top load. The zip-file also contains log-files from server (OSS1). Slab AttachmentLogfiles.zip (70 Downloads) |
7/26/2007 1:40 PM | |
Posts: 1275 Rating:
|
Hi, Have you tried opening this faceplate under APDIAG? It may help you check for errors... There are several errors in your logs.... such as: 26.07.2007,10:58:53:257,1007005,4,ES1,,SCRIPT,Fault in LoadFunktion FaceplateBlockToLoop error: 'FaceplateBlockToLoop': doubly defined function The message "doubly defined function" means that the function has been defined in multiple locations. Go through all the functions and locate and remove the duplicate ones. 21.07.2007,05:53:13:182,1003082,4,ES1,Administrator,NRMS7PMC,MldReceiveMsg: RDFT_EVT_PMC_ALARM8/_ALARM_T Connection CPU_AS36#04, EV_ID 0x00000176: Message overflow detected About this one, check this FAQ. 25.07.2007/05:29:40.928 Channel API error: Error 14 occurred in function 'ChnStartRead' ! 17.07.2007,15:26:03:004,1007006,4,OST1,,SCRIPT,Variable 612_OS_245_Y11$245$a.EventState not exist About this one, check this FAQ. 17.07.2007,15:26:03:004,1007006,4,OST1,,SCRIPT,Variable 612_OS_245_Y11$245$b.QFB_OPEN not exist You should clear those out... Best regards, Danielle |
Last edited by: Danielle at: 26.07.2007 13:56 |
|
7/26/2007 1:49 PM | |
Posts: 3149 Rating:
|
Hi well as I feared, you´ve got some scripting trouble... 26.07.2007,10:09:11:059,1007006,4,OST1,,SCRIPT,Variable 612_PNE_682_WE1.QFB_ON not exist 26.07.2007,10:27:39:464,1007006,4,OST1,,SCRIPT,Variable 612_OS_245_Y11$245$b.EventState not exist 26.07.2007,10:27:39:464,1007006,4,OST1,,SCRIPT,Variable 612_OS_245_Y11$245$a.EventState not exist 26.07.2007,10:27:39:464,1007006,4,OST1,,SCRIPT,10 errors occurs, no more errors will be reported => check your project e.g. via referencelist for not existing tags 25.07.2007,00:37:09:112,1007001,4,OST1,,SCRIPT,ExecuteError in Action @d0ea 25.07.2007,00:37:09:269,1007001,4,OST1,,SCRIPT,ExecuteError in Action @d0eb => http://support.automation.siemens.com/WW/view/en/8385493 17.07.2007,15:07:19:964,1007005,4,OST1,,SCRIPT,Fault in LoadFunktion FaceplateBlockToLoop error: 'FaceplateBlockToLoop': doubly defined function 17.07.2007,15:07:19:964,1007005,4,OST1,,SCRIPT,Fault in LoadFunktion FaceplateLoopToBlock error: 'FaceplateLoopToBlock': doubly defined function 07/25/07 08:37:06 InitLicense CS | AppName = AppCS:Mcp | CycleCheck = yes | NameForMessageBox = | Name = A9WRT130 | License text = SIK/SIMATIC WINCC RT 128 Tags | 07/25/07 08:37:06 NoLicense ED | Name = A9WRC?3? | License text = Simatic WinCC RC (Runtime + Development) | Available = No | 07/25/07 08:37:06 Control Center - Demo Mode Editors turned on - => install your WinCC licenses.. 25.07.2007/06:26:29.382 Connectionerror 2 "CPU_AS36#04": Errorcode 0x0000 7001! 25.07.2007/06:26:29.523 Cannot connect to "CPU_AS36A#11": Errorcode 0xFFDF 011E! 25.07.2007/06:26:29.616 Cannot connect to "CPU_AS36#04": Errorcode 0xFFDF 011E! 25.07.2007/06:27:06.273 Cannot connect to "CPU_AS36#04": Errorcode 0xFFDF 410E! => http://support.automation.siemens.com/WW/view/en/21915653 http://support.automation.siemens.com/WW/view/en/23488713 22.07.2007,17:06:18:291,1003082,4,ES1,Administrator,NRMS7PMC,MldReceiveMsg: RDFT_EVT_PMC_ALARM8/_ALARM_T Connection CPU_AS36#04, EV_ID 0x00000179: Message overflow detected 22.07.2007,20:06:21:822,1003082,4,ES1,Administrator,NRMS7PMC,MldReceiveMsg: RDFT_EVT_PMC_ALARM8/_ALARM_T Connection CPU_AS36#04, EV_ID 0x00000176: Message overflow detected => http://support.automation.siemens.com/WW/view/en/1624059 nemo |
7/26/2007 2:13 PM | |
Posts: 9 Rating:
|
Hi Thanks Nemo and Danielle for replies! Looks like someone have been working on the application after all... Slab |
7/26/2007 2:25 PM | |
Posts: 1275 Rating:
|
Try sorting these errors out, and if you have trouble just post... |
Follow us on