10/24/2017 2:19 PM | |
Posts: 4 Rating: (1) |
Hello, I am installing webserver in my S7-1200 1212C and I want to have a direct access to my web page from the browser (set it as my "Entry page"), but some problems occurred. I can't find any option to do it in TIA Portal V13 sp2. I looked through the forum for some help and someone posted this link: That topic suggests that this solution is for S7-1200 and S7-1500 CPU's, but in my version of TIA-Portal there is no "Entry page" option between "User-defined Web pages" and "Overview of interfaces". In other topic i saw someone who had similar problem and he even posted a photo from his program (in the attachment), but he didn't get the right answer/solution. Maybe I just want too much? Is it even possible to set "entry-page" for S7-1200? Or maybe this is just a problem with my version of TIA Portal? Any kind of help will be appreciated. AttachmentmyTIA.docx (171 Downloads) |
10/25/2017 9:53 AM | |
Posts: 4 Rating: (1) |
Thank you for answer. Unfortunately I think at this point only direct contact with Siemens Support will help (i hope). I made the most simple web page it can be, and the 95% of code is this "Login section" from the Siemens example. It didn't work. When doing everything like in the instruction (link), without using "Entry page" option (which for some reason I do not have in my TIA Portal), I am getting 2 results: - When I will try to go to my website through the direct link "http://192.168.0.1/awp/index.htm", then my browser is showing me a Login/password information (which is ok), but when I type those data and press "Log in" button I am being redirected again to the main S7-1200 Start web page / User Pages from where i have to click another link to finally get to my www page. It can't work that way. I will try to contact with Siemens Support and if I will get a solution (I hope there is one), i will post it below. |
10/25/2017 10:50 AM | |
Posts: 4 Rating: (1) |
I think i found a solution, but I have to check it (I have to wait for Siemens authorization to download some file). I bought my S71200 1212C in 07.2016 and it has 4.1.3 version of firmware. It looks like in 09.2016 (2 months later) Siemens made an update to version 4.2 which should solve my problem: "New features in the V 4.2 release: [...]
Here is a link to this information -> link The newest version of firmware is 4.2.1. I am waiting for the authorization (which i mentioned above) to get this file and I will let you know if it will work. |
This contribution was helpful to1 thankful Users |
Follow us on