11/29/2023 12:13 PM | |
Joined: 5/22/2013 Last visit: 11/13/2024 Posts: 49 Rating: (0) |
Don't Worry! :) "You are not alone" :) :) :)
Finally after following many descriptions and trying 1000different things I have the RT computer running, and a Client PC can log to and check the WEB page. Help! Does some one have the solution. Here is a screenshot of my Client and Runtime PCs also my Example project for TIA17 Upd.6 NO I can not attach a example project :( ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/30/2023 09:38:10New subject after splitting |
|
11/30/2023 9:42 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (174) |
Hello Icoto, please zip the file, because not all file formats are supported in the forum. Hope it helps! Best regards, |
11/30/2023 11:11 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (174) |
Closed cause question posted twice. The second thread with the subject What can I do when I have no Data is published within the conference WinCC Unified Systems. Best regards, |
Follow us on