9/11/2019 4:23 PM | |
Posts: 1 Rating: (0) |
Hi, I am using an "tp-link TL-WN725N" USB-WLAN adapter with should be supported by linux. The "Simatic IOT2040" Image I use is "example-V2.4.0_RC2.wic". When I plag in the USB-WLAN adapter in to the USB-A-Port, there is no LED-Signal that shows the USB-Adaper is working. Also in the "iot2000setup" Setup is no option to select the "wlan0". Does anyone have an idea what can be wrong. Thanks for the support. --------------- "tp-link TL-WN725N" USB-WLAN adapter not working with the IOT2040 (see below) "Edimax EW-7811Un" USB-WLAN adapter works perfect (with out driver installation) Thanks for supporting ------------------------------------------------------------------------------------------ |
Last edited by: ULR at: 09/11/2019 16:25:51Last edited by: ULR at: 09/11/2019 16:26:55Last edited by: Jen_Moderator at: 09/12/2019 10:11:32New subject after splitting Last edited by: ULR at: 09/17/2019 17:51:10 |
|