5/9/2013 4:06 PM | |
Joined: 5/18/2006 Last visit: 10/21/2020 Posts: 170 Rating: (63) |
See attached FAQ 38855207. However, in the table section 2, OS process objects (license: "WinCC RT PO" [OS], "WinCC RC PO" [ES]), item #2 the number of tags for PCS 7 V8 has changed. My understanding (and also based on some testing) this section should be modified to show 90 tags for PCS 7 V8.0 2. Count (not applicable if this exceeds the number of POs in the 1st count)
Also, see the attached from the PCS 7 V8.0 SP1 Engineering Manual |
This contribution was helpful to1 thankful Users |