7/17/2014 12:16 AM | |
Posts: 7 Rating:
|
I switchedto HSC_1 with I1.0 and ID1000. When the fan is running ID1000 is still geting '0' reading. |
7/17/2014 8:22 AM | |
Posts: 5225 Rating:
|
Hi Guys.. may I jump in? Which firmware version are you using for this project? It will help us if you could send us a copy of your program.. make a program where you only us the HSC. Please look at the topic [LINK]. Focus on the files left on 6/28/2014, 3:51 PM and 6/29/2014, 8:48 PM. Please understand the processes explained there before looking at 6/29/2014, 7:20 PM and the discussions following. Is it possible for you to toggle the input slowly at first to see if the counter value? Monitor the physical input on the watch table.. see if it goes on and off. Check again the counter value. Before connecting to a high speed signal.. please make sure that the input is set to the appropriate filter level. By default it is set to 6.3ms (?). You will see this setting under the PLC hardware configuration under the INPUT/OUTPUT configuration for the CPU. Please let us know it this helped. w |
Follow us on