2/5/2019 11:49 AM | |
Joined: 2/1/2019 Last visit: 1/4/2024 Posts: 31 Rating:
|
Need help. The OPC Scout cannot to display any tags from CPU. Only empty folders. The situation: CPU 1214C DC \ DC \ Rly, analog and discrete modules. WinCC RT Professional (128 PowerTags) v14 sp1 update3, WindowsServer2016, TIA Portal v14 sp1 update3, WinCC Professional and STEP 7 Basic v14 sp3 update 3 There is a project: 1cpu, WinCCRT Professional 14, PC station - the OPC server is added to the PC station (the Device configuration already contains the IE general (192.168.1.2) and WinCC RT Professional 14) - an S7 connection is created from the OPC server to the PLC (there is already an HMI connection between WinCC and CPU) Attachment0-02-05-2e2e3e4afce47df8a8ffa576a46af680d7235e7a5f13dd6fcbe81c4487e8b24e_9379db12.jpg (433 Downloads) |
Last edited by: 4phh at: 2/5/2019 11:50:44 AM |
|
Follow us on