3/1/2022 11:06 AM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi,
The Example Image V1.2.1 does not work on the IOT2050 on which you are running the Industrial OS V2.x. That's because of the firmware version. More info see here. The Example Image V1.1.1 does work and it would boot from SD card when you use mmc0 as first boot device (e.g. fw_setenv boot_targets mmc0 usb0 usb1 usb2 mmc1) That would be the easiest step to reach your goal, as the s7 nodes are pre-installed there. For instruction using the Example Image see here. Let's try that at first, I don't want to confuse you more by answering the your other questions with my questions.. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
3/2/2022 9:20 AM | |
Joined: 2/3/2022 Last visit: 3/9/2022 Posts: 14 Rating: (0) |
hi, it works sometimes the solution is very simple thanks for your help
|
This contribution was helpful to1 thankful Users |
Follow us on