9/2/2021 5:17 AM | |
Joined: 8/25/2021 Last visit: 7/15/2022 Posts: 11 Rating:
|
Addition: I just tried to install the node S7 from the source code. I downloaded it as a zip and unzipped it into a folder named "node-red-contrib-s7". Then I copied the folder to the path "/usr/lib/node_modules" and reboot. Subsequently, I opened the nodered in the browse, there is no S7 node. And I checked the "Manage Palette", the S7 node exists, but an error is present: "Error: Cannot find module '@st-one-io/nodes7' (line:42)". So how can I solve it? Best regards! |
10/8/2021 1:08 PM | |
Joined: 9/22/2021 Last visit: 10/19/2021 Posts: 5 Rating:
|
HI Yes, I am using an industrial operating system on EMMC, thank you for your answer |
Follow us on