8/17/2017 7:16 AM | |
Joined: 10/17/2011 Last visit: 7/19/2022 Posts: 148 Rating:
|
Hello Pegaia, I have V14 SP1 and trying to communicate Schneider energy meter EM6400 with S7-1500 on Modbus I am not able to communicate and getting error code 8283 Energy meter and PLC configuration Modbus settings are same ie baud rate 9600. stop bit 1, parity even and data bits 8 As I want to read holding registers from EM6400, I moved 4 in "ModbusCommunicationLoad_db".Mode and 0 in Modbus master block Mode input. Data adder for Modbus master is 43915 to read frequency data length 4 and data ptr is P#DB3.DBX0.0 BYTE 8 wher DB3 Is a data blcock with array of int having size of int0 to int 100 please help me to resolve. Thank you, Damayanti ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/17/2017 8:12:25 AMNew subject after splitting |
|
8/18/2017 12:23 PM | |
Posts: 3093 Rating:
|
Hello Damayanti, Regards, |
Follow us on