12/11/2013 5:13 PM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
Hello Ravi, there are some FAQ wich are helpful in this case. 1. Which connector cables are available for connecting to SIMATIC Panels? 2. How do you do an operating system update (OS update) on operator panels? The answer to your question wich cable is needed are in the 1. FAQ. If the control panel at your KTP is password protected i advice you to do a OS update with reset to factory settings via PPI. All information can be found at the 2. FAQ. With best regards |
This contribution was helpful to
1 thankful Users |
Follow us on