6/30/2017 11:50 AM | |
Joined: 2/4/2015 Last visit: 12/28/2024 Posts: 67 Rating:
|
Hi all, Now I want to place an RIO remotely and communicate it from CPU using wireless. So I connected the LAN cable from CPU to wireless modem then from modem antenna is connected. In the RIO side antenna to modem then from modem to IM 153-4. IP of both modems are 192.168.2.10 & 192.168.2.11 IP of CPU is 192.168.2.1 IP of IM 153-4 is 192.168.2.2 I am able to ping both modems from CPU. But not able to ping IM. Also Bus fault is blinking in IM. Kindly help. Regards Surendhar M ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/30/2017 1:35:15 PMNew subject after splitting |
|
Follow us on