11/18/2016 9:31 AM | |
Joined: 3/28/2015 Last visit: 8/25/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following points might help: 1-How can you determine the size of the load memory and main memory of a SIMATIC S7-300/400 CPU? 2-Compress the load memory; When data are compressed, gaps which have developed between memory objects in load memory/RAM as a result of load/delete operations will be eliminated. This releases free memory in a continuous block. Data compression is possible when the CPU is in RUN or in STOP. 3-Which memory cards can you use with an S7-300 CPU? 4-Kindly find the attached file. |
Eng.Mohamed Ibrahim |
|
Follow us on