4/25/2016 10:25 AM | |
Posts: 10 Rating:
|
hello i have a similar problem with the tia portal since i made an update to update 8. i have nothing in the set pg/pc interface and i cant communicate with any controller. can someone help me? ------------------------------------------------------------------------------------------ |
Last edited by: Blue Moderator at: 4/25/2016 10:52:33 AMNew subject after splitting |
|
4/25/2016 11:09 AM | |
Joined: 4/28/2015 Last visit: 2/24/2025 Posts: 10832 Rating:
|
Hello, look to this batch file, for first look inside it to know what it does, it update interfaces, I expect x64 OS. Hope it helps you. AttachmentPG_Interfaces.zip (808 Downloads) |
With best regards... |
|
4/25/2016 11:19 AM | |
Joined: 7/9/2015 Last visit: 3/21/2025 Posts: 4204 Rating:
|
Hi idop, you can also check this FAQ: How do you assign the parameters of the PG/PC interface in general and what is the remedy if the device driver cannot be selected or is not visible? Regards, Towome |
|
|
4/25/2016 11:20 AM | |
Joined: 9/18/2013 Last visit: 2/20/2024 Posts: 203 Rating:
|
Hello, Which windows are you using? 64bit or 32bit? What was you installing? Which software? Have installed multiple software packages on this windows? |
Follow us on