6/8/2009 5:52 PM | |
Joined: 3/21/2006 Last visit: 2/10/2025 Posts: 10239 Rating:
|
Hello Oskar, If you look at Wizard's first link What transfer options are available in the various operator panels?
Can you give more details about your cable? Regards Hristo Mihalev |
6/13/2009 9:53 AM | |
Joined: 5/28/2008 Last visit: 1/29/2025 Posts: 4518 Rating:
|
Hello Oscar, If your problem is to transfer the project from your PG to the TP177A, please see the attched file as it's contains the methods of transfering proect to the TP. Also you can download the manual of the TP177A from here. Please note that if you would like to communicate your controller with this panel using profibus, its max. speed is 1.5Mbps. Regards, AttachmentProjekttransfer_e_C1.pdf (214 Downloads) |
Ayman Elotaify |
|
Follow us on