Industry Online Support
Technical Forum
6/6/2014 1:21 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Every Profibus network can have upto 126 devices ( Each segment ( Seperated by repeaters ) can have upto 31 slaves ). However there are several factors limiting the actual no of devices ( Which may be much lower than these absolute limits ): a) Amount of Data Transfer per device ( Depends upon the Communication profile selected ) - Pl see attachment for details. b)Max I/O area limit of the CPU ( Depends on the CPU Type ) Pl postyour Configuration details here so that exact cause of the problem is determined. Also pl post what is the Profibus Baud Rate and segment length . Hope this helps Cheers Navnag AttachmentSiprotec_Profibus_Communication.pdf (96 Downloads) |
Last edited by: Navnag at: 6/6/2014 1:24 PMThere is no such thing as the last bug in a program |
|
Follow us on