12/13/2018 6:40 AM | |
Posts: 21 Rating:
|
dear fellows i have network having one master and three slave . Slave connecting with master through DP and wireless communication . i got problem communication drop some time for seconds and OB 86 stop the machine can i put some delay in itterupt of OB 86 and OB 82. because drop communication in seconds not harm our machine. best regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/13/2018 8:33:24 AMNew subject after splitting |
|
12/14/2018 8:55 AM | |
Posts: 21 Rating:
|
L #OB86_EV_CLASS // Leaving state my master and slave PLCs are attached with wireless communication through SATEL Module i want to put DELAY IN OB 86 & OB 82 Interrupt . either the master lost or come within time which could be 10 sec no interrupt will occur. diagnostic buffer is attached with this massage. AttachmentDiagnose_11122018.txt (39 Downloads) |
Last edited by: Bukhari at: 12/14/2018 8:58:07 AM |
|
Follow us on