5/6/2016 9:33 AM | |
Joined: 9/9/2014 Last visit: 11/26/2024 Posts: 246 Rating: (40) |
Hello,c.a.teixeira Array elements can also be used, so that the main element of the array data type has been integer. Boolean variables and data types "string", "char", the real data type is not applicable for this. In the window, select the tag, uncheck the "Show ALL" that would select tag. Or change the properties of the object through the script: Dim Rectangle Set Rectangle = HmiRuntime.Screens("NameScreen").ScreenItems("Rectangle_1") Rectangle.Left = 200 'X position
Rectangle.Top = 300 'Y Position |
Last edited by: Unreality at: 5/6/2016 9:35:53 AMLast edited by: Unreality at: 5/6/2016 1:44:40 PMLast edited by: Unreality at: 5/6/2016 1:45:06 PMBest Regards |
|
Follow us on