2/10/2016 7:52 AM | |
Posts: 3 Rating:
|
Greeting everyone which are part of this big helpful community. This is my very first entry in here. Here is the issue.. I would like to read gas flow value from Elster quantometer pulse output via s1200. Pulse output gives 10 impulses for each m3 of gas. Quantometer has two output cell. I want to use the one with "reed switch" on it. At this point I'm at very begining of this project. Do i need some module for convert pulses to 0-24v, or like EtherMeter solution which compatible with both Siemens and Elster. Exact model of meter is "Elster QA 25"(http://www.elstergasdepot.com/qa25-m40-metric.html) and i also found pulse output cable(http://www.elstergasdepot.com/pulse-output-cable-qa.html) for this product. Pulse output schematic is in attachmet Any help would be greatly appreciated.. . |
Follow us on