4/28/2017 10:34 AM | |
Joined: 10/11/2006 Last visit: 4/17/2025 Posts: 6008 Rating:
|
Hello, you have to use "ConfigEpos". 5.2 Mode selection of EPos with SINA_POS General operating conditions The axis is switched on using input bit "EnableAxis" = 1. OFF2 and OFF3 are preassigned 1 using input "ConfigEPos" – and do not have to be written to for operation https://support.industry.siemens.com/cs/ww/en/view/109475044 |
With best regards, |
|
This contribution was helpful to
1 thankful Users |
4/29/2017 11:03 AM | |
Posts: 24 Rating:
|
Hello, Is this a good way to reset the OFF3 bit? since the OFF3 is the 2nd bit of the word, I multiplied the word with 1111111111111011(16#FFFB). |
Follow us on