7/7/2021 10:44 AM | |
Joined: 7/1/2021 Last visit: 2/21/2025 Posts: 1 Rating:
|
I am having problems getting continuous data logging when setting up historical logging to "on demand". I am using a TP700 Comfort panel using the TIA portal. - In historical data the tags are set up as "on demand" under "Acquisition mode" - The tags including the trigger tag are set up as "Cyclic continuous" with 1 sec cyclic time - For the trigger tag the range is set to 0 for lower 1 and 2 for upper 2. The trigger tag is set to 0 when not logging and 3 when logging. - Trigger tag is set to run the LogTag event "on exceeding" The logging is set to log to a csv-file on the usb-port. I was expecting to get a logging entry every second for each tag, but I am just getting one entry for each tag when starting the logging. Please see attached file with snagits from the setup. Appreciate it anyone has any advice on where the problem might be. Thanks AttachmentHistorical data setup.pdf (647 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on