9/12/2019 9:01 AM | |
Joined: 12/25/2018 Last visit: 1/16/2025 Posts: 76 Rating:
|
hi all, we have a machine with siemens plc ET200. the most of the function of machine is not responding. when i tried to connect with pc it showing an error "Online connection could not be established, The connection partner not responding." i am using step 7 v5.5+sp3, and i used Ethernet net cable to connect between plc and pc. when i search for accessible nodes it is detecting the plc and hmi but when i try to upload station to pg its giving error. can anybody help? please Attachmentet200.pdf (741 Downloads) |
This contribution was helpful to
2 thankful Users |
9/12/2019 9:05 AM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating:
|
What are the settings in the "Set PG / PC interface"? |
9/13/2019 12:54 PM | |
Joined: 12/25/2018 Last visit: 1/16/2025 Posts: 76 Rating:
|
here i am attaching the setting what i did. |
Follow us on