3/7/2018 10:17 AM | |
Posts: 4 Rating:
|
Hello, I'm on TIA PORTAL V14. I've two project : - one project for the CPU-F I use shared device for communicate beetween the two project in profinet (For getting to simotion the safety information coming from the CPU-F). I have two network : - One network (IE2-NET) for accessing to the SIMOTION, the touch screen & for remote maintenance access for troubleshooting. Connected to X130 port of the SIMOTION D435-2. --Deleted Link-- - One network (IE1-OP) for the CPU-F, the I/O Bay. Connected to the X150 (LAN) of the SIMOTION D435-2. --Deleted Link-- When i'm on the CPU-F project and connected to the IE2-NET network, i would like to go online for troobleshooting and loading the CPU-F. But it's not working. In Step 7 classic, it was possible to do it without problem when i was connected from IE2-NET network. Someone know what i must do for doing this ? I don't find. There is a parameter to configurate ? Regards, Attachmentimages.zip (24 Downloads) |
Last edited by: c3ndre at: 3/7/2018 10:19:44 AMLast edited by: c3ndre at: 3/7/2018 10:20:19 AMLast edited by: c3ndre at: 3/7/2018 10:24:36 AMLast edited by: Jen_Moderator at: 3/23/2018 1:56:00 PM |
|
3/7/2018 10:24 AM | |
Joined: 5/12/2006 Last visit: 3/25/2025 Posts: 22600 Rating:
|
Hello, what you need is S7-Routing. The problem is that you use 2 projects (why?). So the PLC doesn't know the Routing Information to the other PLC. in this FAQ is described how you configure this between two projects, but i prefer you use both plc's in the same project. https://support.industry.siemens.com/cs/ww/en/view/109474569 Regards Christoph |
This contribution was helpful to
1 thankful Users |
3/7/2018 11:17 AM | |
Posts: 4 Rating:
|
Thanks, i will test this ! I've another question linked to this. In the touch screen, there is a way to see the alarms coming from the CPU-F. Do i need to do the same, with a dummy station in the two project. Or should i create a proxy device ? Because, before switching to full tia portal, we had two project : - one for scout classic - one for the touch screen comfort panel in TIA Portal. So we used a proxy device to communicate the value from simotion to the touch screen. --Deleted Link-- Do we need to do the same for communicate the alarm coming from the CPU-F in the touch screen ? There is a bloc in tia portal named "Diagnostic overview". We would like to use it to bring the CPU-F alarm in the touch screen. The only problem is than the CPU-F is in another project. So i think, we need to do a proxy or a dummy station (like in your link). What do you think ? --Deleted Link-- Thanks for your time, Attachmentpictures.zip (43 Downloads) |
Last edited by: Jen_Moderator at: 3/23/2018 2:07:16 PMDeleted links and added files as an attachment. |
|
Follow us on