5/17/2012 2:03 PM | |
Posts: 303 Rating:
|
some changes means like downloading blocks into plc. Is it possible to change plc user program and download to plc without stopping plc |
5/17/2012 2:10 PM | |
Joined: 8/31/2010 Last visit: 2/3/2023 Posts: 1498 Rating:
|
Hello Saradhi, FYI, the download in RUN facility is not available in STEP 7 v10.5, to be precise it is possible to download blocks in RUN of S7-1200 only from STEP 7 v11 SP2 (also CPU FW should be v2.2 or above). For more details - Download in RUN (S7-1200) |
Last edited by: Ganes10 at: 5/17/2012 2:24 PMmentioned FW version Like it? Rate it! |
|
This contribution was helpful to
1 thankful Users |
Follow us on