6/8/2011 7:40 PM | |||
Joined: 7/7/2010 Last visit: 5/17/2024 Posts: 14751 Rating: (2374) |
To make a change while connected online with the PLC/CPU, you edit online. This saves from having to STOP the PLC to make simple (or even complicated) changes. It also saves the LONG download times with the process down. |
||
science guy |
|||
This contribution was helpful to1 thankful Users |
6/8/2011 7:54 PM | |||
Posts: 2 Rating: (0) |
Hello Thanks: UMENCHO Thanks: huggy_d1.That was the answer. Let me explain the reason for my question: I used the old S7-200. S7-200 has the "Debug -> Edit Program in Run ". To make minor modifications to the PLC logic program running. I can do the same with PLC S7-1200? I am researching on S7-1200 before using it in some project. Thanks |
||
Last edited by: newkrg at: 6/8/2011 7:55 PM |
|||
8/2/2011 7:52 PM | |
Joined: 8/31/2010 Last visit: 5/21/2024 Posts: 1513 Rating: (223) |
Even it is not available with STEP 7 v11 SP1 . Service Pack 1 (SP1) for STEP 7 V11 |
Last edited by: Ganes10 at: 8/3/2011 6:54 AMLike it? Rate it! |
|
8/10/2011 6:32 PM | |
Joined: 6/29/2010 Last visit: 10/27/2022 Posts: 112 Rating: (63) |
Hello gentlemen, Take a look at the news about the new firmware 2.1: |
8/11/2011 1:29 PM | |
Joined: 6/29/2010 Last visit: 10/27/2022 Posts: 112 Rating: (63) |
Yes Ganes10, I'm too! |
12/3/2011 12:12 PM | |
Joined: 8/31/2010 Last visit: 5/21/2024 Posts: 1513 Rating: (223) |
Download in RUN facility in S7-1200 is available (under update v2.2.0 description) from STEP 7 v11 SP2 (Basic / Professional). The S7-1200 CPU needs to have Firmware v2.2.0 or above Steps on How to perform Download in RUN is available here - S7-1200 Download in RUN mode (online edit) |
Last edited by: Ganes10 at: 12/3/2011 5:34 PMLast edited by: Ganes10 at: 12/3/2011 1:22 PMLike it? Rate it! |
|