11/2/2011 2:23 PM | |
Joined: 6/12/2008 Last visit: 7/2/2023 Posts: 29 Rating:
|
SOME BODY KNOW WHY I CAN ONLY READ INPUT STATUS OR COIL STATUS FUNCTION 01 AND 02 WITH A CP341 RS485 MODBUS SLAVE? I HAVE A CP341 RS485 MODBUS SLAVE AND IAM USING MODSCAN32 SOFTWARE IN MY PG LIKE A MASTER, BUT WHEN I TRY TO READ AN HOLFING REGISTER OR INPUT REGISTER IS NOT POSSIBLE, I CAN READ COIL AND INUTS BUR REGISTERS NOT IS POSSIBLE. IF I MONITORING THE BLOCK FB80 APPEAR ERROR W#16#005C AND THE ERROR INFO W#16#1E0F, I LOOKING FOR THESE ERRORS IN MANUAL BUT ONLY SAID Error when executing a RECEIVE/FETCH call with FB7 (RCV_RK) AND SAID TO RESOLVE THE ERROR: Analyze FB7-STATUS I DONT KNOW WHAT ARE HAPPENING. TO FUNCTION 03 06 AND 16 IAM USING A DB8 AND TO FUNCTION 04 I USE DB9. FOR THESE DB`s I HAVE TO DECLARATE SOME SPECIAL VARIABLES OR ONLY I DECLARE THE WORD I WILLUSE (FOR EXAMPLE REGISTER 40001 - DB9.DBW0. REGISTER 40002-DB9.DBW1, AND SO ON). AttachmentMDBS SLAVE R.zip (137 Downloads) |
11/2/2011 3:17 PM | |
Posts: 93 Rating:
|
Which slave are u using?????? |
11/10/2011 5:25 PM | |
Joined: 6/12/2008 Last visit: 7/2/2023 Posts: 29 Rating:
|
THANKS THE PROJECT IS RUNNING |
This contribution was helpful to
1 thankful Users |
Follow us on