2/3/2014 12:23 PM | |
Posts: 20 Rating:
|
Hi all I Want to Have redundancy on Ethernet but I have 1 CPU. Is it possible? Wich CP is suitable for this. |
2/3/2014 2:25 PM | |
Posts: 20 Rating:
|
It is Network redundancy. with 2 switch.2 Server. 1 PLC 412 . You can see configuration in the attachment. what do you suggest? |
2/3/2014 2:44 PM | |
Posts: 1368 Rating:
|
Hello ali, maybe the Network redundancyPRP (Parallel Redundancy Protocol) with the SCALANCE X204RNA PRP (EEC), SOFTNET IE RNA and CP443-1 RNA. is a solution for you An application example is here http://support.automation.siemens.com/WW/view/de/78790945 More Informations are e.g. here http://support.automation.siemens.com/WW/view/de/49078072 |
2/5/2014 8:59 AM | |
Posts: 20 Rating:
|
Thank you it is ok How I can get Simatic net software? I Can't see CP 443-1 RNA in HW. I upload it but it does n't Exit in my HW. I have same problem with CPU 414-5H. |
Last edited by: ali.riazati at: 2/5/2014 9:03 AM |
|
2/5/2014 9:41 AM | |
Posts: 1368 Rating:
|
hello, the software you find here http://support.automation.siemens.com/WW/view/de/57989518 for the use of the CP, you need the newest hardware support package http://support.automation.siemens.com/WW/view/de/23183356 Good work... |
2/6/2014 8:08 AM | |
Posts: 20 Rating:
|
Thanks, I got S7 SP3. it is ok. I can't find Download link for Simatic net software or SOFTNET-IE RNA. Could I download it? |
Follow us on