12/12/2008 9:09 AM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating:
|
HI, did you mean with "RJ45" a Ethernet cable? You need a crossed Ethernet cable, if you have adirectly connection between PC and Panel. For communicate to a S5 PLC look to this FAQ and the further information in this FAQ -> http://support.automation.siemens.com/WW/view/en/21923974 regards, |
12/12/2008 9:41 AM | |
Joined: 3/21/2006 Last visit: 2/10/2025 Posts: 10239 Rating:
|
Hello Yes you can transfer your program with Ethernet connection. About the cable follow The Brain's advice. More about supported connection you'll find in manual TP 277, OP 277 (WinCC flexible) (page 113-114). And I am afraid that to connect with S5 PLC you'll need to add to your S5 system IM308 module and connect OP277 through Profibus DP (RS485). regards |
Last edited by: UMENCHO at: 12/12/2008 9:42 AM |
|
Follow us on