9/7/2011 9:47 AM | |
Joined: 4/24/2006 Last visit: 2/7/2025 Posts: 8839 Rating:
|
Dear S7-FreshMan, Here is link to manual: OP27, OP37 Operator Panels See chapter 9 Not possible to log on Server PC. Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
9/7/2011 9:52 AM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating:
|
so it can´t be programmed with wincc flex ??? Do i have to use Protool? |
9/7/2011 11:26 AM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating:
|
as far as i have found information about migration to wincc flexible ,it isn´t that easy . /tf/WW/en/Posts/42250 Does all versions of Protool support this OP37,OP37/PRO? Thanks for the information ! :) |
9/7/2011 1:16 PM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
There is a manual about the migration from ProTool to flexible with all needed information: SIMATIC HMI WinCC flexible 2008 WinCC flexible 2008 Migration You need a ProTool/Pro version to project and open a OP37 Pro. |
9/12/2011 12:46 PM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating:
|
Any idea which panel replaces the OP37 or whic panel can replace the OP37 ? |
Follow us on