10/23/2014 3:59 PM | |
Posts: 3609 Rating: (29) |
Import of a question from user chandu@vmsk
|
10/23/2014 5:12 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello chandu@vmsk You know the right password? Try with Admin and password 100 |
10/24/2014 4:31 AM | |
Posts: 18 Rating: (0) |
helloSte39, thanq for reply, i know the correct password. if i try with AD and password 100, it is showing "invalied password of user name login has failed"
|
10/24/2014 7:18 AM | |
Posts: 18 Rating: (0) |
HelloSte39, when i use ID as Admin and password as 100message is displaying
user 'Admin' has unsuccessfully attempted to log on 3 times in succession |
10/24/2014 9:04 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, Your problem is the same of this thread? Have a look: OP 77B Invalid password |
10/24/2014 9:56 AM | |
Posts: 18 Rating: (0) |
thanq for replySte39, yes my problam is same in the thread
|
10/24/2014 10:07 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hi chandu@vmsk, You can try what Ayman says (I never tried), but you need Wincc Flexible and ProSave, you have this software? |
10/24/2014 10:50 AM | |
Posts: 18 Rating: (0) |
haiiSte39, i dont have the software, how i'l get that both the softwares thanks ®ards, chandu
|
10/24/2014 11:33 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello chandu@vmsk, This is Prosave for free, Servicetool+SIMATIC+ProSave - Siemens Industry Online Support ... For Wincc Flexible sorry but you need the license, you have to contact your Siemens department near you. In WinCC Flexible you will find Prosave also. FYI: Pay attention, if you not have have the original project you can't edit the project Look there: OP77A panel with wincc flexible 2008 |
Last edited by: Ste39 at: 10/24/2014 11:44 AMLast edited by: Ste39 at: 10/24/2014 11:44 AMLast edited by: Ste39 at: 10/24/2014 11:40 AM |
|
10/24/2014 12:59 PM | |
Posts: 18 Rating: (0) |
haiiSte39, thanq for reply, i dont want to edit project, is demo version supports for backup and restore? in OP77a ther is no "backuptaranfer" OPTION then how to take backup from HMI thanks®ards, chandu
|
10/24/2014 3:12 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello chandu, The only way is to make upload of project (only backup) you can not edit, andrestore on the same type of panel is using Prosave the link I posted in the previous post. How do you backup/restore with a Windows-based panel? The problem is that I do not know if doing a backup with ProSave and retransfer into the same panel the password will be reset sorry I never tried look chapter 7.3.3 at page 116: SIMATIC HMI HMI device OP 73, OP 77A, OP 77B ... - Siemens Read carefully this thread: Panel password doubts - Siemens Industry Online Support ... and another thing that I forgot since you do not have any software, so I think that you do not even have a cable connection between PC and OP77A: Which connector cables are available for connecting to SIMATIC Panels? |
Last edited by: Ste39 at: 10/24/2014 3:40 PMLast edited by: Ste39 at: 10/24/2014 3:16 PMAdd thread |
|
10/25/2014 9:56 AM | |
Posts: 18 Rating: (0) |
helloSte39, thanq, i will check all d files and i will try. thanq
|
10/25/2014 10:00 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hi chandu, Tell us the result |
10/26/2014 11:15 AM | |
Posts: 18 Rating: (0) |
helloSte39, i tryed to complete backup from the HMI PANEL, but it is showing the "error during synchroniazation or incorrect device celected" im using PC/PPI cable, i'm attaching the screen shorts what the error is displaying, please help me for further thanks & regards, chandu
|
10/26/2014 12:13 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hi Chandu, Tell us the complete part number of your PC/PPI cable If you have this PC/PPI cable look fig.11
|
Last edited by: Ste39 at: 10/26/2014 12:49 PM |
|
10/27/2014 5:44 AM | |
Posts: 18 Rating: (0) |
helloSte39, ther is not any serial number on cable, it is SIEMENS CABLE S7-200(PC-PPI) PRINTED on labul, im attaching the cable picture, my doubt on baudrate setting in prosave general tab, when i select OP77A two baudrate values are availabul 57600 and 115200, witch one i hv to select? and corresponding this is we need to do any changes in device manager port settings in pc? thanks & regards, chandu
|
10/27/2014 8:50 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello chandu, I do not think the cable seen in your photo be able to connect to the panel, you need one of these cables: What transfer options are available in the various operator panels ... |
10/27/2014 9:40 AM | |
Posts: 18 Rating: (0) |
thanqSte39, i want to buy new cable, http://www.ebay.com/itm/6ES7901-3CB30-0XA0-Cable-RS232-to-RS485-PC-PPI-for-Siemens-S7-200-PLC-Optical-/170929949220 may i use the above cable for OP77A with PROSAVE ? thanks and regards, chandu
|
10/27/2014 5:32 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hi chandu, Sorry for the delay, For me with this cable there is not a problem. |
10/28/2014 4:42 AM | |
Posts: 18 Rating: (0) |
thanqSte39, i am ordering the cable, after i receive the cable il try and update the result thanks and regards, chandu
|
This contribution was helpful to1 thankful Users |
Follow us on