1/1/2014 10:47 AM | |
Posts: 1 Rating:
|
Dear Sir/Lady We have an intractable problem with an OP77A with the order No. 6AV6641-OBA11-0AX1. Its Version Info is: 01.03.00.00_08.34 BL 1.8/2006-11-22 The problem is that after power up we can readily select serial transfering mode and transferingstarts in this mode very easily without any trouble.But if we disable serial transfering and enable MPI/DP transfering, as soon as we press Enter to start transfering , OP goes into suspension mode (Hanged up) and consequently no one of its buttons work properly. The only possible way to reset OP from this, is to unplugging 24 VDC 1-Is connection to ProfiBus networkmandatory before starting DP Transfering ? 2-Does Operating system have any influence on this issue? Thanks In addvanced |
Last edited by: AutoGen_433345 at: 1/6/2014 10:28 AMLast edited by: AutoGen_433345 at: 1/1/2014 10:49 AM |
|
1/7/2014 11:34 AM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
Hello AutoGen, 1-Is connection to ProfiBus networkmandatory before starting DP Transfering ? No is isn´t. 2-Does Operating system have any influence on this issue? Maybe yes, maybe not... to this question i haven´t got a real answer. Because of this i advice you to start a support request at the technical support, because it isn´t a normal attitude. >> Support Request With best regards |
Follow us on