8/20/2015 10:35 PM | |
Joined: 10/17/2007 Last visit: 4/22/2024 Posts: 3972 Rating: (340) |
I have m/c using OP77B, when booting I can only see the screen light--seem back light is ok. but no any menu or text display. it happened last week. it working good for 4 years. 'Can any one tell me, I need order the new OP77B . or how can I recover my old OP77B. PS: I have no WinCC flexible, only have Pro Tool/ Pro Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/21/2015 9:01:44 AMNew subject after splitting If you like my comments please |
|
8/20/2015 11:25 PM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, 1-OP77B programmed with WinCC flexible. 2-I think you not able to upload the program from the panel in your case. Servicetool SIMATIC ProSave3-you should have a copy of the program of the panel or program the panel from the starting. 4-try to perform: How do you do an "Operating system update" (OS update) or "Reset to factory settings" on operator panels?5-If you not success to repair OS,So the panel damaged and should be repaired or replaced with a new one and need to download the program to it. |
Eng.Mohamed Ibrahim |
|
8/21/2015 1:08 AM | |
Joined: 10/17/2007 Last visit: 4/22/2024 Posts: 3972 Rating: (340) |
Thanks for quick answer. I think I cannot repair this OP by myself, As I have no WinccFleixble nor SIMATIC ProSave, I only have SIMATIC Manager and Pro Tool/Pro in my Laptop. Luckily I found one spare OP77B in our stock which we ordered from m/c builder years ago, and it is pre-loaded oem program inside, I just connected it then everything working OK. We will order another OP77B from m/c builder with pre-loading program, PS: m/c is made in Germany , and we have good relation with them for years, they should support us.
|
If you like my comments please |
|
This contribution was helpful to1 thankful Users |
8/21/2015 10:35 AM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, Iam happy that you solved your problem but I advise you when you order this panel from the M/C builder to order a copy of the panel program. |
Eng.Mohamed Ibrahim |
|
8/21/2015 10:38 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, If you want Prosave please or above by Online Tech: Servicetool SIMATIC ProSave - Services - Siemens |
8/22/2015 8:10 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello nulizhang, #1 - I think is for this:
#2 - What transfer options are available in the various operator panels? |
Last edited by: Ste39 at: 8/22/2015 8:13:41 AMLast edited by: Ste39 at: 8/22/2015 8:14:56 AMAdd # for point Last edited by: Ste39 at: 8/22/2015 8:29:50 AMLast edited by: Ste39 at: 8/22/2015 8:30:36 AMCorrect link Last edited by: Ste39 at: 8/22/2015 8:39:41 AMCorrect link |
|
8/22/2015 11:01 PM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hell, My advice for making the communication between PC/PG and OP77B panel is to use RS 232 cross cable as in the attached file "it is simple and cheap". |
Eng.Mohamed Ibrahim |
|
Follow us on