11/18/2018 10:52 AM | |
Joined: 8/22/2016 Last visit: 3/10/2025 Posts: 40 Rating:
|
Hello Aden, ad 1: the OPC server feature is nowadays in every S7 1500 CPU. It is possible to activate it in the settings of CPU and then select appropriate licence version. The size of the OPC license depend on the type of PLC used (details you can find in industry mall or in the TIA selection tool). Of course legaly it is mandatory to buy the OPC license, if you are going to use it, anyway for test purposes ... ad. 2: I personally didn't try it in the PLC sim, but in details of PLCSIM advance you can find, that OPC UA functionality is supported, so I suppose, it is functional. Regarding the PC application... I did the similar application last year and I can recommend the application example from Siemens - see this sample. Regards Josef |
Follow us on