7/14/2022 7:03 AM | |
Joined: 9/3/2008 Last visit: 4/11/2025 Posts: 933 Rating:
|
Hi lucasribas First, it is important to know if the type of OPC server you want is Classic OPC DA or it is OPC UA DA? Also, what cpu type do you want to access and is the DB optimized/non-optimized? If it is a 1200/1500, optimized DB then this could be the reason you are not able to access the datablock variables. In that case you need to use OPC UA server. Regards |
Michael |
|
7/14/2022 3:26 PM | |
Joined: 9/14/2021 Last visit: 3/4/2025 Posts: 14 Rating:
|
I enabled only COM/DCOM configuration, as it shows on the image. |
Follow us on