Industry Online Support
Technical Forum
7/1/2009 6:27 AM | |
Posts: 691 Rating:
|
may be this link will help you http://www.tsopc.com/documents/opcspec/opcda20_auto.pdf?PHPSESSID=fe889a13454612b4d9b3dd8fd5cc18fb#search=%22DataAccess%20Automation%20Interface%20Specification2%22 |
7/1/2009 7:39 AM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating:
|
Hello Lalit, Perhaps this example is helpful: How do you create an OPC client with Microsoft Excel?. How can i connect to Siemens PLC's via VBRegards Hristo Mihalev |
Last edited by: UMENCHO at: 7/1/2009 7:45 AM |
|
7/1/2009 8:19 AM | |
Posts: 487 Rating:
|
You need to have a ethernet card in the PLC ( 443-1) then you can communicate via sockets to the PLC , on the PLC side you would use the AG_Send ( FC5) and AG_Recv (FC6) from the comm library. Have a look at this link it's the quick start CD for all comms things .You can use a normal ethernet card on you PC .You also don't need the siemens NET stuff .But you do need a TCP or UDP component In Delphi I use a component from 'indy socket' according to the website it can be used with VB. Hope this helps you Eric |
7/2/2009 3:11 AM | |
Joined: 12/20/2008 Last visit: 7/18/2024 Posts: 556 Rating:
|
the link is not working |
7/2/2009 7:13 AM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating:
|
Hi, I can't open only Ninja Robot' link. I already sent to him PM to check his link and if it is possible to repair it. Mine and Eric' links work. Regards, Hristo Mihalev |
7/2/2009 7:25 AM | |
Joined: 12/20/2008 Last visit: 7/18/2024 Posts: 556 Rating:
|
OK. I will wait for Ninja's link to get open. Thanks.for your links too. |
Follow us on