Industry Online Support
Technical Forum
11/29/2008 12:17 AM | |
Posts: 3 Rating: (0) |
Hi folks, 1) After i set OPC connection, i want to test via OPC-Scout but my groups and items does not occur under "\SYM". "\SYM" is empty so i do not catch my variables which i specified as input or output at code side... In addition, below document points that OPC groups and items should be occurred under "\SYM"... http://support.automation.siemens.c...iew/en/17490972 How can i solve this problem? 2)How can the information be transfered from the TEMP data to M or DB? Regards, Eren |
12/2/2008 11:41 PM | |
Posts: 5822 Rating: (412)
|
Dear Eren, I wonder, what do you see if you try to select the Symbols? Do you see anything there? Please post a Screenshot if possible. Best regards J_Bell |
Follow us on