10/17/2007 2:09 PM | |
Posts: 1776 Rating:
|
Hi, maybe some DCOM Settings are missing See FAQs http://support.automation.siemens.com/WW/view/en/24201837 http://support.automation.siemens.com/WW/view/de/24201837 http://support.automation.siemens.com/WW/view/de/22892718 When an OPC client accesses a WinCC OPC server via a network, from OPC DataAccess 2.0 onwards a query is sent to the OPCEnum first to determine whether there is an OPC server available and, if so, which. If the OPCEnum is not configured on the OPC server, two DCOM messages are entered in the Windows event viewer. OPCEnum has to be configured just like your OPC server. You can find out about configuring this in the WinCC Information System, section on "Release Notes > Notes on WinCC > WinCC Runtime > OPC Communication". The settings for the DCOM application are shown there. |
10/17/2007 4:06 PM | |
Posts: 36 Rating:
|
Thanks April It solved the problem. Strange why the WinCC installation does not configure this automatically, it should do this!!! |
Follow us on